2024-08-23 10:20 PM
Hi
Can someone head me in the right direction to locate a very basic project to use a ST25 together with one of the HID chips or similar: Project for a tag only read direct into spreadsheet via HID. Thanks Charles
Solved! Go to Solution.
2024-08-27 6:26 AM
Hi,
for your specific need of having an ID for each reader, I would suggest you contact those solution providers. PC/SC NFC readers may also fit your needs.
Rgds
BT
2024-08-26 1:17 AM
Hi,
If my understanding is correct (please correct me if I am wrong), you want to develop a project with an NFC reader connected to a PC through USB and be able to read some data from an NFC tag directly into a spreadsheet.
Which NFC technologies do you plan to support (NFCA and/or NFCB and/or NFCF and/or NFCV)?
Have you had a look on STEVAL_25R3916B or ST25R3911B-DISCO? or to existing products such as FEIG CPR30/30+?
Rgds
BT
2024-08-26 6:16 PM
Hi Brian
Yes you are correct. Available at the moment are usb stick for readding of rfid, but they do not have a user ID for each reader.
I would like the simplest easiest way to read to spreadsheet with alreaddy available components. Would try an Arduino option if feasible. But i thing there will be some chips that can be used to get it working. All I need is read tag only, and attach ID to the data going into spreadsheet.
Thanks
Charles
2024-08-27 6:26 AM
Hi,
for your specific need of having an ID for each reader, I would suggest you contact those solution providers. PC/SC NFC readers may also fit your needs.
Rgds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.