2019-11-14 6:58 AM
Hello,
I am curious if there is a RFID reader that extends the communication distance for STEVAL-SMARTAG1. If so, could you kindly provide the link and description.
Thanks in advance,
J.X
Solved! Go to Solution.
2019-11-19 5:10 AM
Hello,
First of all, thanks for your interest in ST smartag product !
If the communication distance reached with ST NFC HF readers is not sufficient for your application you can have a look at FEIG readers such as LR1002 for example
Hope this helps,
Best Regards,
BB
2019-11-19 5:10 AM
Hello,
First of all, thanks for your interest in ST smartag product !
If the communication distance reached with ST NFC HF readers is not sufficient for your application you can have a look at FEIG readers such as LR1002 for example
Hope this helps,
Best Regards,
BB
2021-04-23 1:48 AM
Dear, I have got in touch with FEIG and they told me that none of their products can handle the STEVAL-SMARTAG1 protocol. Could you please recommend another company? see below the message from FEIG.Good afternoon,
-----------------------------------------------------------------------------------------------------------------------------------
Thanks for your request and we a the distributor of FEIG Electronic will inform you.
I looked at the specifications of this tag and this one does not support the protocols the FEIG readers support. The FEIG readers support ISO14443, ISO15693 (HF) and GEN 2 (UHF) so in this case they are not able to read the tag.
Met vriendelijke groeten, Best regards,
Arnold Zweep
Inside sales
Duranmatic B.V. - Auto-ID
+31 (0)78 65 31 872 - auto-id@duranmatic.nl
2021-04-23 4:12 AM
Hi JSant.5,
I can only imagine a misunderstanding here:
STEVAL-SMARTAG1 uses ST25DV. ST25DV is an ISO15693/NFC-V tag so supported by the Feig reader.
Regards, Ulysses
2021-04-23 4:38 AM
Dear Ulysses,
OK many thanks for the information, I will then contact them again, probably indeed there was a misunderstanding.
Regards,
Juan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.