2016-04-26 4:18 AM
Hello,
I'm currently starting to add the CR95HF to one of our projects and I'm not sure, which library is recommended to use.The project itself is using the STM32-HAL drivers for hardware access (and it should stay this way!). The controller is a STM32F071 and the interface is SPI.The whole thing gets a bit more interesting, as we are going to connect 2 CR95HF to the chip - so ideally the library *should* support this (or should be easy to switch between 2 chips).What I've found so far:Is there anything else I should take a look at?
Any other suggestions?Thanks in advanceMarcoSolved! Go to Solution.
2016-07-01 1:59 AM
Hello Marco
You could have a look to the software package which is developed for the nucleo expansion board (X-NUCLEO-NFC03A1, based on a CR95HF). The software environment is based on STM32 Cube, and intended for a STM32F103 or STM32F401. Hope this will help you. Have a nice day. kind Regards2016-07-01 1:59 AM
Hello Marco
You could have a look to the software package which is developed for the nucleo expansion board (X-NUCLEO-NFC03A1, based on a CR95HF). The software environment is based on STM32 Cube, and intended for a STM32F103 or STM32F401. Hope this will help you. Have a nice day. kind RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.