2022-11-15 10:34 AM
Hello,
In the x-nucleo-nfc08a1 reference design, there is the standard 3 variable cap setup (2 series, 1 parallel) plus also a second set of parallel vari-caps (C307 and the oddly named 4C30). But these are not populated on the board. Should we populate these in custom designs? In my design the antenna is a PCB trace coil about 0.75" in diameter but the trace length is about 10 inches and goes through a relay.
Thanks,
Derek
Solved! Go to Solution.
2022-11-16 12:34 AM
Hi Derek,
please see AN5322 chapter 5 for a discussion on usage of VCCs and different schematics.
BR, Ulysses
2022-11-16 12:34 AM
Hi Derek,
please see AN5322 chapter 5 for a discussion on usage of VCCs and different schematics.
BR, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.