2025-03-06 1:37 AM
This might be *** question but I have to ask as as I'm a biginner... I want to interface ST25r3916 with STM32F072xx without using BSP package and HAL. I'm currently using bare metal embedded c. I've been trying to change rfal_Platform.h file which I think I got right. is it possible to write the code from scratch since the example code is generated by MXCube??
Solved! Go to Solution.
2025-03-06 3:36 AM
Hi,
no problem to use the RFAL without STM32 HAL. RFAL was ported to various systems from small 8-bit up to Raspberry Pi userspace Linux.
BR, Ulysses
2025-03-06 3:36 AM
Hi,
no problem to use the RFAL without STM32 HAL. RFAL was ported to various systems from small 8-bit up to Raspberry Pi userspace Linux.
BR, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.