2025-03-06 7:49 AM
I'm in trouble using dll with c# for using the mailbox.
Can someone help me?
Please @Ulysses HERNIOSUS , my friend, help me! I'm pain too!
Here is the code:
private void TxRxNBytes_Click(object sender, EventArgs e) {//This is a button click event handler
sbyte[] rx = new sbyte[512];
//Here following is the reversed uid byte sequence compared to the one reported from software ST25PC-NFC
byte[] uid = [0x61, 0x92, 0x74, 0xD0, 0x01, 0x24, 0x02, 0xE0];
ee = ST25R391x_Dll.iso15693Select(Handle, uid); // ee=NoError
sbyte[] tx = { 0x10 , unchecked((sbyte)0xAA) , 0x02 , 0x06 , 0x01 , 0x02 , 0x03 , 0x04 , 0x05 , 0x06 };
ee = ST25R391x_Dll.iso15693TxRxNBytes(Handle, tx, 10, rx, ref uRxDim, 1); // ee=NoError...
// ... but microcontroller hosting ST25DV04K doesn't receve the GPO signaling.
// Instead, using software ST25PC-NFC -> Fast Transfer Mode -> WriteMessage , the microcontroller hosting
// ST25DV04K hit an interrupt due to MB_CTRL_Dyn -> RF_PUT_MSG and reading the mail box results the
// exact sequence {0x01,0x02,0x03,0x04,0x05,0x06}
What i'm doing wrong?
Can someone help me?
Solved! Go to Solution.
2025-03-06 8:16 AM - edited 2025-03-07 4:08 AM
Hi,
what are the values of the GPO and GPO_CTRL_Dyn registers? is the Write Message (0xAA) command successful, if not, what is the return code? Be aware that "MSGlength" parameter of the command is the number of Data bytes minus 1 (see §7.6.31 Write Message in the Datasheet). So, the MSGLength should be 05 for "01 02 03 04 05 06"
Rgds
BT
2025-03-06 8:16 AM - edited 2025-03-07 4:08 AM
Hi,
what are the values of the GPO and GPO_CTRL_Dyn registers? is the Write Message (0xAA) command successful, if not, what is the return code? Be aware that "MSGlength" parameter of the command is the number of Data bytes minus 1 (see §7.6.31 Write Message in the Datasheet). So, the MSGLength should be 05 for "01 02 03 04 05 06"
Rgds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.