2019-05-07 12:04 PM
Hello!
I am starting my activities with the Demonstration Board MB1054A CR95HF and according to what I understand it is only possible to write in a block of 4 bytes, I wonder if there is how to write in only 1 byte?
Detail: mine NFC tag is ST25DV04K.
Regards,
João Pedro, Engineering Student from Brazil.
Solved! Go to Solution.
2019-05-07 3:10 PM
Hi João Pedro
the physical memory of an ISO/IEC 15693 tag is organized in blocks (or pages) of fixed size (see ISO/IEC 15693-3 §5 VICC memory organization). Therefore, the various read or write commands follow this memory organization (e.g. Write Single Block command)
If you want to modify only one byte:
Also I would suggest you use the STSW-ST25PC001 Windows® PC software. It supports the CR95HF demo board and provides menu to read and write tag memory. It supports as well features of the ST25DV04K.
Rgds
BT
2019-05-07 3:10 PM
Hi João Pedro
the physical memory of an ISO/IEC 15693 tag is organized in blocks (or pages) of fixed size (see ISO/IEC 15693-3 §5 VICC memory organization). Therefore, the various read or write commands follow this memory organization (e.g. Write Single Block command)
If you want to modify only one byte:
Also I would suggest you use the STSW-ST25PC001 Windows® PC software. It supports the CR95HF demo board and provides menu to read and write tag memory. It supports as well features of the ST25DV04K.
Rgds
BT
2019-05-08 7:22 AM
Hi BT.
Thanks for your response. All right here... Thanks for the tip, i'm downloading the software.
Regards,
João Pedro.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.