2026-04-09 1:55 AM
Since the 210 reader seems to be cheaper and smaller (in non BGA package) than the 3916b we are currently using, while delivering comparable output power, I am naturally intrigued.
But the wakeup mode figures don't quite impress, even though it is advertised for situations "where each µA matters".
Wake-up mode for the ST25R300, ST25R500, ST25R501 and ST25R210 - Application note
gives a 75.17 μA figure for 200ms scanning (using 250mA Amplitude)
Wake-up mode for ST25R3916/16B, ST25R3917/17B, ST25R3918, ST25R3919B, and ST25R3920/20B devices - Application note
gives a 43.74 µA figure for 200ms scanning (using 200mA Amplitude)
Even adjusted for the amplitude difference, that would give >35% more power draw for the 210. Is there a way this is compensated through higher sensitivity, so actually we need less Amplitude on the 210, or should I really expect a regression in low power card detection?
Solved! Go to Solution.
2026-04-09 2:53 AM
Hi,
these two example numbers cannot be really be compared:
Without having done the math in detail I expect with similar Tmeas and similar amplitude also similar power consumption. Compared to ST25R39xx I expect much more sensitivity.
You can even further reduce Tmeas and see if it affects noise floor and thus also sensitivity.
BR, Ulysses
2026-04-09 2:53 AM
Hi,
these two example numbers cannot be really be compared:
Without having done the math in detail I expect with similar Tmeas and similar amplitude also similar power consumption. Compared to ST25R39xx I expect much more sensitivity.
You can even further reduce Tmeas and see if it affects noise floor and thus also sensitivity.
BR, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.