cancel
Showing results for 
Search instead for 
Did you mean: 

EVB-T5MCM NMEA via Teseo Suite v7.6.3

hoho_city
Associate

I am trying to check RTCM and NMEA data on the EVB-T5MCM, but I have encountered the following issue.

When I run Automatic Port Detection in Teseo Suite v7.6.3, I can only see RTCM data. I tried adding NMEA by selecting the NMEA checkbox in the configuration in order to view NMEA data, but I still could not see any NMEA messages.

The configuration detected by Automatic Port Detection is as follows:

HW Type: TESEO5
Baud Rate: 921600
Data Bits: 8
Parity: None
Stop Bits: 1

What would you recommend that I try next?

0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.