2015-11-17 8:25 PM
I have to integrate NFC into STM32 series controller.
I am able to successfully detect the tag by sending following commands. After successful completion of Select2 process.I send PWD_AUTH commnd as my tag is read and write protected. I get response as 87 00(Frame wait time or no Tag) But my PWD_AUTH command internally it is success and i can get access to read and write into the tag.PWD given is accurate and correct in ascii values. Can you let me know why instead of PACK response i get 87 00 </colgroup>0x02 0x02 0x00 0x00
PCD Field OFF0x09 0x04 0x68 0x01 0x07 0x00 Reset RF
0x09 0x04 0x68 0x01 0x07 0x10
Set RF0x02 0x07 0x02 0x00 0x00 0x00 0x00 0x02 0x02
Protocol Select0x09 0x04 0x3A 0x00 0x58 0x04 PCD WR REG Gain:0x58
0x09 0x04 0x68 0x01 0x01 0xD3 PCD WR REG Gain:0xD3
0x04 0x02 0x26 0x07
REQA0x04 0x03 0x93 0x20 0x08
AntiCol10x04 0x08 0x93 0x70 0x88 0x04 0xBF 0x66 0x55 0x28
Select10x04 0x03 0x95 0x20 0x08 AntiCol2
0x04 0x03 0x95 0x20 0x08 0x04 0x08 0x95 0x70 0x88 0x04 0x0E 0x90 0x77
0x28 Select2
0x04 0x06 0x1B 0x52 0x6F 0x61 0x64 0x28
PWD_AUTHUID: 0x04 0xBF 0x66
0x04 0x0E 0x90 0x77 #ntag213
Solved! Go to Solution.
2015-11-18 12:46 AM
Dear,
if your command PWD_Auth is correct and if your tag responds , (you can check it with a scope and a loop to spy the communication) , CR95HF probably miss the reply because it is out of Max frame delay time , play with PP MM DD parameter to enlarge CR95HF duration of detection window . Regards2015-11-18 12:46 AM
Dear,
if your command PWD_Auth is correct and if your tag responds , (you can check it with a scope and a loop to spy the communication) , CR95HF probably miss the reply because it is out of Max frame delay time , play with PP MM DD parameter to enlarge CR95HF duration of detection window . RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.