2015-09-17 8:27 AM
Hello
I am using an M24LR16E-R eeprom in I2C mode.I have written to the I2C_Write_Lock bits and have set sector 0 as write-protected. Process as follows:Present Password commandWrite I2C_Write_Lock bit (0x0001) //to set sector 0 as protectedI have read the write lock bits afterwards and confirmed that they have been changed. However, when I have tried to write to sector 0, it is still possible to write the memory sector despite the lock bit being set.Have I missed a step? Any help would be much appreciated.CheersDan #m24lr16e #stm32l-m24lr16e-i2cSolved! Go to Solution.
2015-11-13 6:18 AM
Hello Dan,
as far as i know You can write to this sector because You have rights to it from Present Password command. This command remains active until the M24LR is powered off or unit a new I2C present password command is issued. Plese try this and let me know.RegardsPetr2015-11-13 6:18 AM
Hello Dan,
as far as i know You can write to this sector because You have rights to it from Present Password command. This command remains active until the M24LR is powered off or unit a new I2C present password command is issued. Plese try this and let me know.RegardsPetr2015-11-17 6:46 AM
Hello ,
basic sequence is 1) present valid I2C password 2) protect zone by writing correspondant I2C write lock bit this protection will be activated on only after presenting a bad password or after a POR , 3) each time The valid I2C password is presented , sector writing is possible , I2C password act as a Super User . until next POR or presentation of a bad Password .We’re moving the ST Community to a new platform to give you a better and more reliable community experience.