2019-10-25 4:39 AM
We have designed the board for,
Input:
Voltage - 200 to 240 V
Frequency - 50 Hz
Output:
Voltage - 12 V
Ampere - 400 mA (*Considereing the datasheet, the default float design has been approached. Without the use of any Current Limiting resistor)
But unfortunately, Currently
1. We are getting the output of 11 ~ 13 V ( having a 3% error) without a load being connected.
2. When the desired load is added, there is a heavy major drop in output voltage, giving an output of 2 V in fluctuation.
3. The desired/ added load (which is of 100 mA), is unable to receive its required recommended input.
The current from Viper output is ceaselessly being fluctuated, with 15% of output required.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.