Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

When we apply or connect load to Viper26. The output is being dropped from 12 V to 2 V. With current being continuously fluctuating. How do i solve this issue ?

We have designed the board for,Input:Voltage - 200 to 240 VFrequency - 50 HzOutput: Voltage - 12 V Ampere - 400 mA (*Considereing the datasheet, the default float design has been approached. Without the use of any Current Limiting resistor)But unfort...

To limit the OCP of an L6599AD to one function

Hello. I have a question about the okp function while using l6599AD. The daasheet states that the ISEN pin operates in the hiccup mode when the voltage is 0.8V and the shutdown when the voltage is 1.5V. When testing with a regular electronic load, th...

Jyu.6 by Associate
  • 988 Views
  • 0 replies
  • 1 kudos

Hall effect sensor noise

My motor works fine at the first 10 to 20 sec. However, I observed there is some noise spike and the speed feedback error occurs. What would be the problem? I have added 3300pF at the output of hall effect sensor.

0690X00000AqrjhQAB.png
Ysiu by Associate II
  • 875 Views
  • 0 replies
  • 0 kudos

Alternative for TIP31C in SMD Package

Dear Experts,now working for vehicle ignition control through Relay (https://www.conrad.com/p/tianbo-electronics-trv4-l-12v-z-automotive-relay-12-vdc-1-change-over-1366523) , i have attached my circuit and i want to replace the tip31 to any other SM...

0690X00000AqnpCQAR.jpg
Knate by Associate II
  • 1624 Views
  • 1 replies
  • 0 kudos

B-G431B-ESC1 - Fine shaft position control

Hi,In my application, I'd like to control the position of the motor shaft instead of the speed, since I have more than one motor and I want them to move in phase (they are connected and controlled by CAN). I saw this board has the possibility to add ...

bernat2 by Associate
  • 757 Views
  • 0 replies
  • 0 kudos

What is this method of driving BLDC?

Hey guys. We are trying to drive a 350 watt scooter sensored bldc motor.we use common circuits available online and we use gate drivers(ir2103) with 6 n channel mosfets to swith between phases.In every step we pull one phase high and one low and the ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.