2020-05-07 2:23 PM
Hello,
I am working on closing the loop on a system I am designing, and I am not able to determine the transfer function of the the L6591 from any literature you have, and it is not yet supported by your edseign suite software.
I was hoping you could point me to the right right direction as far as the COMP pin input is concerned....is it just a unity gain input? Is there any error amplifier gain/phase changes I need to be aware of, or is all that accomplished by the recommended external compensation circuit?
Also, I am planning on utilizing this chip in a full-bridge implementation by having the drive outputs drive opposing legs of the H-bridge, do you see any problems arising from this method as the chip is marketed for half-bridge implementation?
Thanks so much,
Tim
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.