Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HALL_MAX_PSEUDO_SPEED question

HALL_MAX_PSEUDO_SPEED questionat HALL_TIMx_CC_IRQHandler() function, how come the "if condition" become TRUE, then assign HALL_MAX_PSEUDO_SPEED value to pHandle->CurrentSpeedI found that the motor is not rotated, but the HALL_M1.CurrentSpeed value is...

cyt by Associate II
  • 726 Views
  • 0 replies
  • 0 kudos

SRC0CS25D fail

I have 3 boards that shares same power input schematic from battery power. I use SRC0CS25D to control power up of board. First two boards works great.The third board works, but the 3 sample which i used for debug purpose, after a while they fail to p...

AGugl.1 by Associate
  • 983 Views
  • 0 replies
  • 0 kudos

SPI interface AD9484 (STM32F765NI)

Hello,we are new on this products.The connection is between stm32f765ni mcu to the AD9484 device under Half-Duplex spi communication.From the datasheet what we understand is the following procedure:HW:First Bit: MSBData Size: 16 BitsBaud RAte: 27.0 M...

MikeS1 by Associate
  • 896 Views
  • 0 replies
  • 0 kudos

Class 1 Accuracy meter ic

I am Anees PK form Riodlogic ,India-Kerala.We have planned to use STPM34 for Energy meter IC to measure the Energy consumption for EV charging stations for the Billing application. So please confirm this IC can provide 1% accuracy on Energy measureme...

APK.1 by Associate II
  • 929 Views
  • 0 replies
  • 1 kudos

Two application questions for powerSTEP01 - how to externally power the core correctly and how to drive brushed DC motors?

1. Power supply to the core logic: What is the right way to do this such that the Vs motor supply can be turned on and off while leaving the logic running? The datasheet leaves much to be desired (which are input power and output power pins is confus...

JMeng.1 by Associate II
  • 3340 Views
  • 7 replies
  • 0 kudos

How to use the VIPER222LSTR IC?

I want develop a power supply board for my STM32 project.For my power supply board I want use a VIPER222LSTR converter but reading the datasheet I realized that some resistors and capacitances values not are specified.How to use the VIPER222LSTR IC?T...

0693W000000WQbRQAW.png
JToni.1 by Associate II
  • 871 Views
  • 0 replies
  • 0 kudos

STWBC-EP, STEVAL-ISB044V1 based design Communication issues

ST,My team and I have designed a Qi wireless Transmitter (TX) based closely off the STEVAL-ISB044V1, sharing the STWBC-EP controller and the overall block diagram. The principle difference is more robust front end protection, (Fuse, zener, RPP, TVS)...

0693W000000WNIRQA4.png
TWuer.1 by Associate
  • 602 Views
  • 0 replies
  • 0 kudos

forward/backward/brake with PWM signal in STEVAL-SPIN3201

Hello all, I'm interested in getting the STEVAL-SPIN3201 for my robotics project.I'd like to know if it's possible to control it with PWM/PPM commands, and if it is, how to perform the connections (it's not shown in the datasheet, maybe when buying i...

Oat.1 by Associate
  • 827 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.