2021-05-30 9:28 PM
I'm using a 694W solar cell whose Voc is 6V, Vload = 5.03V at MPP (Maximum Power Point). Its Isc and ILoad are 160mA and 138 mA at MPP. Under this condition, is it safe to use SPV1050?
2021-05-31 2:08 AM
You probably made a mistake and mean 694mW, right?
Regarding SPV1050: as you can read in the data sheet, the maximum battery charging current is given as 70mA and therefore doesn't fit in your application.
Regards
/Peter
2021-05-31 2:18 AM
Hi, Peter! Thank you so much for your answer.
I'm using a 0.6W solar cell whose specifications are as below
Voc = 6.2V
Vload (Max) = 5.02V
Isc = 147mA
Iload (Max) = 138mA
I am using a 1000 mAh lithium-ion cell as storage. Please let me know should if I can use SPV1040 instead of SPV1050?
2021-05-31 4:37 AM
The SPV1040 should be able to handle this, but please read the data sheet carefully as table 4 lists some precautions, e.g. for output voltages above 4.8V:
According to the absolute maximum ratings the output charge voltage cannot be above 4.8 V but if a higher VOUT up to
5.2 V is needed, a Schottky diode must be placed between the Lx and VOUT pins as shown in Figure 1. In such way the
Schottky diode in parallel to the embedded P-channel MOSFET reduces the voltage drop between the VLX pin and the
VOUT pin determined by the body diode when the internal PMOS is OFF from 0.7 V down to 0.3 V.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.