2026-04-09 2:29 AM
Hello,
In the STPMIC datasheet, the BSTOUT continous current is specified as being greater than 1.1 A when 3.3 V < VIn < 5.5 V.
If the voltage Vin is greater than 4.5 V, does the BSTOUT continous current increase?
I assume so, since the inductor's peak current limit (IBSTLIM) is 3.3 A and the short-circuit current (IBSTSH) is 4 A, but could you confirm this for me?
If so, what is the BSTOUT continous current when Vin>4.5 V?
Best Regards.
Sylvain
Solved! Go to Solution.
2026-04-09 2:51 AM
Welcome @SB_arrive, to the community!
No - a higher continuous BSTOUT current cannot be assumed just because VIN > 4.5V.
There is no separate rating or curve for higher VIN in the data sheet, so the continuous BSTOUT current is still only guaranteed as min 1.1A. To take worst-case conditions into account, therefore, a higher current should not be assumed either.
Hope that answers your question?
Regards
/Peter
2026-04-09 2:51 AM
Welcome @SB_arrive, to the community!
No - a higher continuous BSTOUT current cannot be assumed just because VIN > 4.5V.
There is no separate rating or curve for higher VIN in the data sheet, so the continuous BSTOUT current is still only guaranteed as min 1.1A. To take worst-case conditions into account, therefore, a higher current should not be assumed either.
Hope that answers your question?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.