Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to use internal opamp in stspin32f0602

I have been using stspin32f0602 based on evspin32f0602s1. But the evaluation kit uses external opamp and comparator ic. I am looking for a way to use the internal opamp and comparator for amp measurements for easier hardware and inventory management....

Fkadr.1 by Associate II
  • 1359 Views
  • 1 replies
  • 0 kudos

VIPER26L compatibility with VIPER26K

Hi, we are using VIPER26LDTR in a non-isolated AC/DC converter with 220V AC line input and 16V DC output. Can we replace the chip with VIPER26K version without changing the circuit/PCB? The K version has a MOSFET capable to withstand 1050V but apart ...

GGrec.1 by Associate
  • 876 Views
  • 0 replies
  • 0 kudos

Resolved! How to drive the BOOT pins of a STSPIN32F0251?

I have an EVSPIN32F02Q1S1 board to experiment. Each boot pin has a connection to Vcc via a diode (D1, D4, D7) - which are not mounted on the board. When driving a phase full on the pull up MOSFET breaks down about every 2.5ms. The time varies dependi...

MLamp.2 by Associate
  • 1144 Views
  • 2 replies
  • 0 kudos

H2PAK-2 vs H2PAK-6 MOSFET package for high current application

I'm using multiple MOSFET of STH310N10F7 in parallel for current of approximately 60A.MOSFET are used in DC Bias and not switching so time delay is not a factor of consideration.I'm confused between the packages.What are intended application of H2PAK...

SJain.3 by Associate
  • 3075 Views
  • 1 replies
  • 0 kudos

Beginners question: IHM01A1 + Stepper - What am I doing wrong

I am an owner of the STEVAL-EDUKIT, an inverted pendulum kit by ST with an NUCLEO-F401RE, IHM01A1, Nema17 motor and an rotary encoder + a 2A, 12V power supply. I have no prior experience with motor control whatsoever. See https://www.st.com/content/s...

MDaub.1 by Associate III
  • 1257 Views
  • 0 replies
  • 0 kudos

IHM01A1 Shield project - How to create from scratch?

I am using a IHM01A1 Stepper motor shield with an STM32F401. The provided example for one motor from the X-CUBE-SPN1 package works as expected and I can properly control the motor.Now I want to basically recreate the project from scratch as a prober ...

MDaub.1 by Associate III
  • 828 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.