2023-04-26 12:12 AM
I am looking for alternate for VNS3NV04D-E, please confirm VNS3NV04DPTR-E is suitable alternate? what is buying source & manufacturer lead time.
2023-04-26 12:29 AM
Welcome, @VMali.1, to the community!
Yes, the VNS3NV04DPTR-E can directly replace the obsolete VNS3NV04D-E, the parameters are identical. However, it is your responsibility to re-check any necessary approvals.
No one in this technical forum can give you a source of supply, so please contact your local distributor.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
2023-04-26 5:07 AM
2023-04-26 5:17 AM
Not really - the only dual low side switch being a bit similar is the VNLD5090-E, but its current limit is much higher. You can buy it directly from estore.st.com.
Good luck!
/Peter
2023-04-26 11:34 PM
VNS3NV04D-E is tube packaging with NRND & VNS3NV04DPTR-E is tape & reel with Active status, can we consider VNS3NV04DPTR-E with 6-8 year life span..
2023-04-26 11:37 PM
also same for VNLD5090-E is not active for purchase link VNLD5090TR-E is available. Please confirm. End of life for VNLD5090TR-E also
2023-04-26 11:39 PM
VNS3NV04DP-E is not in the Product Longevity program, so long-term availability cannot be guaranteed or stated.
Regards
/Peter
2023-04-26 11:40 PM
VNS3NV04D-E is tube packaging with NRND & VNS3NV04DPTR-E is tape & reel with Active status, can we consider VNS3NV04DPTR-E with 6-8 year life span?.
also same for VNLD5090-E is not active for purchase link VNLD5090TR-E is available. Please confirm. End of life for VNLD5090TR-E also?
2023-04-26 11:48 PM
VNLD5090TR-E as active and in full production. It is also not part of the Product Longevity program, so long-term availability cannot be guaranteed or stated either.
As already mentioned, this is a technical forum. For statements on stock availability, please always contact the respective supplier/distributor, as stock can change daily.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.