Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STPM32 Interrupt pin behaviour

hello,I do have a question about the INT1 pin behaviour of the STPM32.I measured all pins with a saleae logic pro 16 and decoded the spi communication also.From the beginning, the initialization routine looks as described in the datasheet.It is at le...

0693W00000aInT7QAK.png
ARose.6 by Associate
  • 1439 Views
  • 2 replies
  • 0 kudos

Using STPM34 voltage channel as current channel

I am designing a power metering circuit using the STPM34 IC, and I need to measure three channels of current. The STPM34 datasheet specifies that the device has two current measurement channels (IP and IN) and two voltage measurement channels (VIP an...

Resolved! Serial Number, Unique ID available on interface for powerStep01

For a project using several powerStep01 drivers it would be very useful, if each powerStep01 could be identified by a unique ID or a serial number. In the interface description no such register is defined. Is there maybe a hidden register available w...

pf8645 by Associate II
  • 2711 Views
  • 4 replies
  • 0 kudos

[STSPIN32G4]The footprint of STSPIN32G4(VFQFPN 9X9X1.0 64 PITCH 0.50)

hi When confirming the footprint of STSPIN32G4(VFQFPN 9X9X1.0 64 PITCH 0.50), we find that the length of STSPIN32G4 =4.10+2.03*2+0.85*2=9.86(STSPIN32G4 - High performance 3-phase motor controller with embedded STM32G4 MCU - �?法�?�导体STMicroelectronics...

TT.6 by Associate
  • 842 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.