2025-10-30 4:06 AM
Hello,
I'm considering using Viper12 to 3Phase AC/DC non isolated buck converter 5V 60mA Vout. I found some application notes like AN1357. But is it reliable? Or will it cause problems in long-term operation? Has anyone experienced it before?
Thanks,
Gökhan
2025-10-30 6:05 AM
Welcome @MGökhan, to the community!
First, a note: the AN1357 is already obsolete and has long been unavailable online (at least on our website).
Although you did not specify the value of your 3-phase voltage, assuming a voltage of 380V, you will not be able to use a controller with buck technology. The reason for this is that with your low output power of 0.3W, the controller would have to have extremely short switch-on times in order to regulate effectively, which such controllers are not designed for. In addition, in this voltage class, a regulator with a maximum reverse voltage of 1050V, such as VIPER265K, would have to be selected, but this is also not suitable for your application.
In your case, a flyback regulator will work most reliably. On the one hand, it requires a transformer, but on the other hand, it can work without any problems with regulators such as the above-mentioned VIPER265K.
Hope that helps?
Regards
/Peter
2025-10-30 6:27 AM
2025-10-31 6:58 AM
You still haven't mentioned what the effective value of your input voltage is or what the maximum value of the rectified 3-phase voltage is. Without this information, I'm assuming 380Vac or 540Vdc.
The outdated AN1357 you uploaded refers to a buck converter with a single-phase mains voltage of max. 265Vac and a larger load. In this configuration, such a non-galvanically isolated design can certainly work. The eDesignSuite from STMicroelectronics can also simulate such single-phase designs – but only for reasonable voltage and load ranges.
If your 3-phase voltage is 380Vac, such a buck converter is not feasible for your very low output voltage of 5V, as I explained earlier.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.