2023-11-25 4:48 AM
Hello,
I'm using TCPP03 for a DRP solution. For my design it would be good to use the Mosfet drivers for controlling a logic input for further power control instead of using Mosfets. Is it possible to use the gatedrivers with the SRC-pins connected to Ground and feed the GATE-Pins to an input of a logic device? I'm aware that I have to take care for the logic level translation.
I did already tests and it worked so far. Just to get safe that there will be nor furhter impacts, I want to know your suggestion for this.
Regards
Michael Houzer
Solved! Go to Solution.
2023-11-27 8:39 AM
Hello Michael,
Your case is clear and TCPP03-M20 match to your needs.
To rephrase, TCPP03-M20 SOURCE and SINK gate drivers must drive logical levels.
SOURCES are connected to the GND.
GATES (5.0V output voltage) can be connected to :
There is no TCPP03-M20 restriction for this case.
Best regards,
Mathieu
2023-11-27 8:39 AM
Hello Michael,
Your case is clear and TCPP03-M20 match to your needs.
To rephrase, TCPP03-M20 SOURCE and SINK gate drivers must drive logical levels.
SOURCES are connected to the GND.
GATES (5.0V output voltage) can be connected to :
There is no TCPP03-M20 restriction for this case.
Best regards,
Mathieu
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.