Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! TCPP03-M20 using Mosfet driver outputs for logic control

Hello,I'm using TCPP03 for a DRP solution. For my design it would be good to use the Mosfet drivers for controlling a logic input for further power control instead of using Mosfets. Is it possible to use the gatedrivers with the SRC-pins connected to...

mikeho by Associate
  • 1484 Views
  • 1 replies
  • 1 kudos

steval-L99615C GUI not working

Connected discovery board to COM port. Using Demo bin file, have been able to view data with serial monitor. When I connect using Unicleo GUI 1.25.1.11665, COM port message states successfully opened. Unable to view any other data. Firmware: Expansio...

KWarr.1 by Associate II
  • 1241 Views
  • 2 replies
  • 0 kudos

Resolved! L6924D Battery charger NTC selection

I require assistance with the design of the battery charger schematics involving the L6924D. Referring to the documentation (https://www.st.com/resource/en/datasheet/l6924d.pdf), the pull-up resistor R3 is 1K, and the NTC tuning resistor R9 is 470 oh...

l6924d.png
Levan by Associate III
  • 2216 Views
  • 2 replies
  • 1 kudos

Resolved! SMD marking V20

May i know what is the part number for this parts.  

1700710096517.jpg
wcs00 by Associate
  • 2442 Views
  • 2 replies
  • 3 kudos

STSPIN840 OUTX1 and OUTX2 signals

Hi,We have PCB where STSPIN840 is connected to PIC32MK1024MCF100 and DC motors connected to respective OUTX pins. Getting PWM,PH(high),EN(high) when we are checking signals in CRO but OUTX1,OUTX2 both as 3.3v or one 3.3v another 12v sometimes. Accord...

KTH by Associate
  • 875 Views
  • 0 replies
  • 0 kudos

STEVAL-ASTRA1B Low-power

Hi. I am currently evaluating the STEVAL-ASTRA1B as a low-power LoRaWAN-GPS tracker. My goal is to have the device wake up every 10 minutes to send a GPS position.I am however facing some problems getting the current consumption down to the advertise...

NikkoSTM by Associate II
  • 992 Views
  • 0 replies
  • 0 kudos

SCTHS300N75G3AG Sic POWER MOSFET Rds(ON)

Hi all,   In SCTHS300N75G3AG Sic power MOSFET data sheet mentioned that 8.8mΩ Rds constant over maximum temperature. But in graphs Rds(on) reached to above 1.3mΩ. So, which value we need to consider for power dissipation calculation.

Rds on.png graph.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.