2019-05-03 7:11 AM
Hello friends,
I made a custom STSPIN32F0 board , copy all sames STEVAL-SPINS3201 except STM32F103 side ,
We upload default software from motor library and system works well in EVM SPINS3201 but when we upload same software to our boards , there is no movements,
When we checks registers, system stuck in FAULT_OVER or IDLE mode, system not turn to RUN mode
What is the problem can be? we checked all board , there is no difference with EVM board
Any idea?
2019-05-13 12:36 PM
Hello,
Do you have an UART connection with your board ? If yes are you able to connect with motorcontrol workbench ?
Did you check that your code reach the while loop in the main.c ?
Regards
Cedric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.