Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
Also, there are many source code modules provided in the software download, but there doesn't seem to be any explanation of which modules to compile to run the BLDC controller.
I'm using steval spin3202 board and want to implement a Foc based bldc motor control driver with hall effect sensor.Please help.
For a test application I require up to 8 A of current (although at a lower voltage), is it wise to use multiple of these evaluation boards in parallel. To prevent shoot-through, a small ferrite bead/inductor can be used in series with the driver, but...
Hello,where I can find any documents related OTP programming on this IC?Many thanksAndrey
On page 44/75 of the L6470 Datasheet it says "The available range is from 0 to 0.996 x VS with a resolution of 0.004 x VS, as shown in Table 12."I am using an ElectroCraft motor (TPE17-32A20-1100-0) which has a Voltage (V/Phase) = 2.2.So if I want a ...
Hi everyone, I am new to the community and I am also not very expert on microcontrollers. I own a STM32F407G-DISC1. I was able to write the code for ADC (at least I think), but I don't know how to save the data on the memory. Can anyone tell me how t...
when:VDD=SD=IN=PWM=12VVoltage between OUT1 and OUT2 is +40mVDirection of OUT1-OUT2 voltage flips depending on DIRThis happens when driver supply voltage (VS) is disconnected or VS = 12V , 24V, 48V .I'm guessing that the output driver of PWD5F60 is si...
i want to control AC voltage using firing angle control for this which ic gives rising edge at exactly zero crossing point of ac sine wave op-amp or optocoupler?
TwisterSIM becomes unstable after second simulation. Plotter interface hangs and becomes unusable... Got to close whole program and start again. (Win7)Anyone knowing about that trouble ? Workaround ?Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.