2021-07-05 1:12 AM
Hello, Could any body tell me the maximum input current of Analog pin (VIP, VIN, IIP, IIN)? From the datasheet i can only find the maximal analog pin Input voltage with -0.7 to 0.7V.
2021-07-12 10:00 AM
Welcome, @YCai.2, to the community!
Due to the high input impedance of 8Mohms, these analog inputs should never have any significant current flowing into them.
Do you need this parameter to protect the device?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.