2014-01-08 2:07 PM
Hi to all, my name is Cosimo and I need help about stepper driver.
From an old printer I've get a bipolar stepper and now I'm trying to drive it with L298 and L297 configuration. Whitout the stepper the output of L298 are: 0V 12V 0V 12V. It's ok! But with the motor the output of L298 are: 6V 6V 6V 6V. Why this?Testing the L297 output I've without the motor: pin 4 0V, pin 6 4.4V, pin 5 4.4V, pin 7 0V, pin 9 4.4V, pin 8 4.4V.
Testing the L297 output I've with the motor: pin 4 0V, pin 6 4.4V, pin 5 2.2V, pin 7 0V, pin 9 4.4V, pin 8 2.2V.
Thanks in advance.Cosimo #l298-l2972014-01-11 2:11 PM
solved! 6V are normal in stepper when the start condition is 0101 with 12V supply of stepper.. the problem was ground connection between boards (driver L297+L298 and PIC32 starter kit) and clock speed to high.. thanks to all.
2014-02-20 7:21 AM
I am an Electrical Engineering student. I just wanna ask whether is there any need to connect optoisolator with L298? Doesn't it has built in protection?
I am using STM32F303 microcontroller with NXT lego motors. Specs of motors are:Stall current: 2AFree running current: 60mA2014-02-24 2:08 AM
Hi,
Usually optoisolator are not required in this kind of applications. The L298 integrates thermal protection and the current ratings you indicated are within the safety ranges of the IC.EnricoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.