2014-02-11 3:59 PM
Hi,
Is there an online version of the BEMF compensation tool? I have a couple of boards from Sprakfun that are based on the L6470 but I'm having issues getting the performance out of the stepper motors that I thought I would be able to get. Maybe I'm a bit dense but looking at the BEMF formulas I'm getting numbers that are ridiculously high so I must be messing something up somewhere. If there isn't an online version of the tool could someone possibly walk through an example of the calculations? That way I could see where I'm going wrong and be able to apply the same calculations to other motors that I have as well. Thanks #l64702014-02-12 5:11 AM
As an example this is what I am currently getting as a value based on the BEMF formula:
INT_SPEED = 4 * Rm/2�?€Lm * 2^26 * ttick where ttick == 250nsMotor specsRm = 1.65Lm = 2.8Im = 1.68INT_SPEED = (4*1.65/(2*pi*2.8))*(2^26)*250 =6293988307.48
Does this seem correct? Any of the other posts I've seen about INT_SPEED they seem to be using much lower numbers.Thanks2014-02-17 7:34 AM
Hi,
I think you forgot the order of magnitude of some of the parameters. Inductance is expressed in mH and the tick time is in ns: INT_SPEED = (4*1.65/(2*pi*2.8*10^-3))*(2^26)*250*10^-9 =698830748
In any case you can use the attached document for the calculation of the parameters. Best Regards Enrico ________________ Attachments : BEMF_compensation.xlsx : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzI1&d=%2Fa%2F0X0000000bJM%2FXBYEO0lVfnTTdcR_klKHkTpFRhcgDFrEslLENaIewO4&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.