2021-11-14 11:45 PM
Hi, the output pins of the STCMB1 (pin 14 ,16,19) that drive the mosfets gate are protected from transient current peaks ?
In the datasheet there are the current capability of the drivers (e.g pin 14 GD_PFC is capable of a 0.6 A source current and a 0.8 A sink current).
If I put a very low external gate resistance (1-2 Ohm) , when the mosfet turn on the driver output peak current theoretically exceed the 0,6 A source current of the datasheet.
The STCMB1 is internally protected from that istantaneous current peak ? it automatically limits the driver current to 0,6 A ?
Or otherwise I have to design the external gate resistance of the mosfet to guarantee that the maximum driver current is lower than 0,6 A also during that transient ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.