2014-07-22 12:47 PM
I have used EVAL6482H board to drive a stepper motor with a spec as followed,
Operating voltage: 2.5v
Rated current/ phase: 0.49A
Supply voltage: 20v
I set the parameter as followed
Stepper.setParam(TVAL_HOLD, 0x02);
Stepper.setParam(TVAL_RUN, 0x02);
Stepper.setParam(OCD_TH, 0x08);
Stepper.setParam(CONFIG, 0xF788);
Stepper.setParam(GATECFG1, 0xC7);
Stepper.setParam(GATECFG2, 0x61);
Stepper.setParam(T_FAST, 0x47);
Stepper.setParam(TON_MIN, 0x07);
Stepper.setParam(TOFF_MIN, 0x1F);
However, the return value from getStatus is 0xE403 ( 1110 0100 0000 0011), which indicates the undervoltage lockout and the flag LED keep winkling.
Can anyone help me to find out the problem?? Thank you.Grace2014-08-21 5:16 AM
Dear Grace,
the configuration looks ok. Please, consider the following: - at power up the device always returns an UVLO failure - after you change the VCC_VAL value from 7.5V to 15V there is a transition time required to assering the new supply voltages at the VCC and BOOT pins, during this period the UVLO failure is triggered - Check if the BOOT and VCC voltages are ok. Kind Regards EnricoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.