Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6470 Stall detect issue

Posted on July 24, 2014 at 15:26Hello, I am posting this question that another user posted but there was no answer. Can anyone help?Can't reliably sense stalling using L6470 chipI've been quite successful at controlling the L6470 stepper driver chip...

msmith by Associate II
  • 1261 Views
  • 1 replies
  • 0 kudos

Problem for EVAL6482H

Posted on July 22, 2014 at 21:47I have used EVAL6482H board to drive a stepper motor with a spec as followed,Operating voltage: 2.5vRated current/ phase: 0.49ASupply voltage: 20vI set the parameter as followed   Stepper.setParam(TVAL_HOLD, 0x02);   ...

ywliao by Associate
  • 1054 Views
  • 1 replies
  • 0 kudos

Current readout circuit problem!

Posted on August 17, 2014 at 10:32Gigi or Dino:        I met a strange question, motor parameter in STM3210E+ MB495 successfully entered the closed loop control. Now I redesign custom board,      The open loop mode debugging hardware correctly, when...

BLDC motor control at 60000 or more RPM

Posted on July 03, 2014 at 12:06We are working on a Medical Respirator equipment, for which we need to control the BLDC motor up to 60,000 RPM. To generate a speed of 60000 RPM, Space Vector Modulation PWM waveform main/base frequency shall be 4 KHZ...

prashant by Associate II
  • 2727 Views
  • 6 replies
  • 0 kudos

V/Hz control of an ACIM

Posted on July 01, 2014 at 16:16Hi, I would like to control some small 3 Phase Induction motors with means of an analogue input and a potentiometer. I am looking at a V/Hz (Scalar) library that I could use with an ST processor. Can someone direct m...

cdtsilva by Associate
  • 1162 Views
  • 1 replies
  • 0 kudos

STM32 SVPWM modulator

Posted on July 20, 2014 at 15:17Hello, I am looking for solution of SVPWM implementation for STM32F103 microcontroller. My application is AC motor frequency converter with U/F = const regulation. Best regards Andrzej #stm32 #3phase-motor #frequen...

FOC Control and Resolver input

Posted on July 29, 2014 at 18:04Hi, I have a PMSM which I'm planning to run sensor-less. In case I run into problems with the sensor-less the motor I'm using also has a resolver fitted. I have a Resolver Decoder from analog devices so I'm wondering...

L6470 step loss A (or B)

Posted on July 21, 2014 at 23:12i've been using the L6470 driver successfully but have noticed that i get step loss on the a and b bridge. the data sheet indicates that when this happens the appropriate bits in the status register get set. unfortuna...

spelger by Associate II
  • 892 Views
  • 1 replies
  • 0 kudos

L9958 SPI control

Posted on July 22, 2013 at 15:39The question is related with the command word under the SPI protocol title. In this protocol uC should sent the command word to start protocol but I can not find the structure of this word. In datasheet the CFG_REG an...

hozsarac by Associate
  • 2530 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.