2015-06-09 10:01 AM
Hello,
I just wanted to know the required current capacity for VH and VL for EVALSTGAP1S. I am using it fior SiC , VH=20V and VL = -5V.2015-06-10 4:26 AM
Hello Mr. Morya,
As far as I understand, with using the SiC MOSFETS something between 2A and 5A should be okay. The STGAP1S has a max capability to support 5A as maximum. The rest depends on your MOSFETS, in this case the SiC(?). KrWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.