2014-04-22 5:31 AM
Hi,
We have an application with a small steppermotor with only a small load. the current and voltage we use is way too high for the motor for longer periods of time, we only use it in short bursts. The problem is that we cannot set the acceleration of the L6472 high enough. our stroke is only 2 turns and it never gets to its maximum speed. Is there a way to increase the 'Tick' speed? 25 - 50% would be ideal for us. Thanks, Remco #l6470-l6472 #l64702014-04-24 5:57 AM
Hi,
It is not possible to change the tick time value. If you want to bypass the limits of the integrated motion engine you shoud use the step-clock mode. Regadrs Enrico2015-02-25 6:43 AM
What is the maximum allowed frequency for the clock step mode (L6470, 128 uSteps)? Does the back EMF compensation work in this mode? If so, it would mean that the chip somehow measures the frequency and adjust the phase amplitude accordingly, right?
2015-03-04 10:57 AM
Remco,
ST employees seem to know nothing about this product. I have the same application, a 40 oz*in NEMA 17 motor with a 3 oz*in inertial load and 1 step/second rate, intermittient, then up to 7200 s/s. It is not possible to achieve that speed range with a fixed power supply on the L6472 board. The main problem is the supply voltage and that youre probably using too high of a current level, and its the wrong board. Do this: 1. Use the 6472 and set the Accel - Decel and Run currents equal, and at a very low value like 250 mA. Set the motor voltage to between 8 and 10Vdc for single step, or around 17V for 100 s/s, or choose a motor voltage value based on the V/Hz test to measure phase voltage at the desired step rate. Then choose the minimum operating currents that allows the motor to step. Then add a little current to make it stable. 2. Use the L6470, it is much more advanced than the 6472 and controls phase voltage and current (it controls phase current through controlling phase voltage unlike the 6472 which is a current limit scheme with fixed motor voltage.) If the motor voltage is too low in either case, the motor cannot accelerate up to speed, may set an OC alarm and apparently that is what youre seeing. You can do that, it just takes getting support and ST refuses to support us. Sad./We’re moving the ST Community to a new platform to give you a better and more reliable community experience.