2018-02-26 6:16 AM
L6472 stepper driver.
hello, we are using 4x L6472 driver chip on a single board for some time now. We used the internal 16MHz clock, but it appeared that the clock frequencies differ a lot from each other. According the specs it can be plus or minus 3%. With four motors running simultaneously, it looks a bit funny to see them running different speeds/s. So what we did is using an external clock source. This clock is generated by the attiny, so is only available after the tiny is up and running. This worked for a coupe of days.
now my question; this morning we blew up ( housing cracked open) 3 of the 4 L6470 while programming the Attiny. And we want to know why that happened? Also the boot diodes of three L6472 fried.
Is this because the L6472 needs a clock before it can handle the init strings via SPI? I cannot find anything in the spect about the external clock and/or/if it must be present before the L6472 receives serial data?
Or, is there an other reason why three drivers fry? where to look at?
regards,
rob
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.