2025-09-23 7:37 PM - edited 2025-09-23 7:38 PM
Hi Sir,
Would it be feasible to achieve an 80A peak current on this board simply by modifying the OCP circuit hardware and the corresponding firmware settings in X-CUBE-MCSDK? Or will thermal constraints and the PCB design itself (e.g., trace width, layout) prevent this from being a viable solution?
( This is considering that the Power MOSFET used on the board, the STL160N4F7, has a much higher pulsed current rating according to its datasheet.)
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.