2025-09-22 1:44 AM - last edited on 2025-09-22 1:52 AM by Peter BENSCH
Dear,
please advice me.
Balancing not working.
Used Steval board with J13, J14 and all J5 open (disconnected) .
HS mode.
3 cells connected (C5-C4-C3) and (C2-C1-C0-GND)
Used test script:
| WRITE | 6 | 0AD8 | N=10, Cell OV = 4.21632V |
| WRITE | 7 | 0A33 | N=10, Cell UV = 0,99552V |
| WRITE | 8 | 0A0A | Severe Cell UV = 0,8V, Severe Cell OV = 4.41152V |
| WRITE | A | 0AE2 | N=10, VB_OV = 22,0576V |
| WRITE | B | 0A2D | N=10, VB_UV = 4,392V |
| WRITE | C | 16 | VB Sum Max Diff = 1,0736V (0B) 1,464V (0F) 2,14 (16) |
| WRITE | D | A000 | N=10, NTC OT = 0V |
| WRITE | E | AFFF | N=10, NTC UT = 3.30057V |
| WRITE | F | 1 | NTC Severe OT = 3.30057V |
| WRITE | 10 | FAFA | test má byt 0x13 pro 2,2 A ( 1313) |
| WRITE | 11 | 00FA | test persistent OVC TH 2,2 A |
| WRITE | 9 | 0A05 | bal_delta |
| WRITE | 1 | 007C | CHR DCHR Balancer |
| WRITE | 4 | 1AFC | Enable 3 cells, VB, & NTC measurement proud |
| PAUSE | Press OK to begin voltage acqusition | ||
| WRITE | 2 | 07FF | Start acquisition. Filter times set to max - Tmeas_cycle = 150ms |
Everything seems to work fine but balancing not
What am I doing wrong?
Will balancing affect charging or discharging or both?
Thaks you very much
Pavel
Solved! Go to Solution.
2025-09-23 9:43 PM
I'll answer myself
L9961 does not balance automatically by itself. Balancing must be controlled by the MCU. The value of register (0x01) 0x007C is nonsense. It must be 0x0060.
2025-09-23 9:43 PM
I'll answer myself
L9961 does not balance automatically by itself. Balancing must be controlled by the MCU. The value of register (0x01) 0x007C is nonsense. It must be 0x0060.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.