2024-11-08 9:42 AM - last edited on 2024-11-08 10:42 AM by Peter BENSCH
Hello,
The AEK-POWBMS63EN is a Battery Management System. I am not sure if I can connect to a voltage lower than 48V, if yes, would it work optimally? What issues I might come into?
Please kindly advise
2024-11-08 10:46 AM
The description is a little misleading, the 48V refers to a single block consisting of up to 14 Li-Ion cells, which have a maximum total of 48V. You can of course also charge one single cell.
Hope that answers your question?
Regards
/Peter
2024-11-08 12:12 PM
Thanks Peter for responding!
So what does the 800V mean?
2024-11-10 1:08 PM
800V means many blocks (nodes) in series, each one with a dedicated L9963 able to handle 4…14 Li-Ion cells.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.