2014-05-11 1:57 AM
I'm evaluating L99ASC03 to control a brushless motor which drives a propeller.
A series of LiPo accumulators will supply the board. The supply voltage is about 7V when 2 LiPo accumulators are used. When more LiPo accumulators are used, supply voltage increases up to 25 V in 3.7V steps. This supply voltage range matches the L99ASC03 internal +5V voltage regulator limits, but it may waste too much power when many LiPo are used. Is it possible to connect the +5V output of a switching regulator to the VSREG input while VS and VSMS are directly connected to the LiPo accumulators? Regards EtaPhi #bldc-motor-control #l99asc032014-05-14 3:25 AM
Hi EtaPhi,
it is possible to implement your configuration. Best regards, Marco2014-05-14 4:12 AM
Thanks, Marco!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.