2013-05-09 1:12 AM
I put in a technical support request on this but no response.
I'm running a Viper16 in a simple non-isolated buck configuration as per the data sheet. There is a spark ignitor on the board and sometimes when the spark occurs, the Viper16 shuts down. I can understand it might go into one of its overload conditions but it does not recover. Vdd sits at 12V, 0.25V on FB and 0V on LIM and COMP. If I inject current into Vdd, the Viper16 starts again. Strange. Has anyone had this sort of problem with the Viper16 or other Viper chips?2014-05-20 7:41 AM
Hi, I have a similar problem with the Viper26HN,
We do Surge testing on the board and the viper stop working, the output is at 0.38V, FB+Comp at 0.1v, and VDD a 13.5V. I need too kill the main input voltage for 10-20sec for the viper to restart. Any solution ?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.