2025-03-23 7:14 PM - last edited on 2025-03-23 11:51 PM by Peter BENSCH
EN_EL pin (#47) is originally EN function and to set it as RST function, need to set D[4] of reg8Ah.
My question: When to set D[4] to 1 to enable RST function? should it do after setting watchdog ?
Thanks!
RST Remapping on EN_EL the function of Input reset pin. (Configurable via
SPI at 1st start-up, stored in PROM). Enabled via SPI (EN_EL_RST_EN,
reg8Ah/138d D[4])
Watchdog
Programmable fault limit count (SPI_set_WDfailLimit)
Programmable overflow timer (SPI_set_WDtime)
2025-03-27 8:15 AM
Hi @haihun
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.