Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MC34063ACD-TR

Hello Anyone did ever you use the MC34063ACD-TR for to power on a "MCU" at 3.3V? From datasheet it seems it needs change R1 and R2 for to obtain the goal but the figure 15 shows until 5V so..I ask you if i can use it for my application. My applicatio...

STWLC99 cannot connect to GUI

我的WLC99RX开发板无法连接到GUI,我下载了wlc_ft260_Recovery这个文件,我连接了STEVALUSBI2C,但是并没有用,可不可以给我一个详细的教程。我还有一个问题是解释我的GUI界面似乎与开发板手册上的展示的不一样,GITHUB网页已经404,请问可以通过邮箱发给我与手册上展示一样的GUI软件吗,谢谢 Translation: My WLC99RX development board cannot connect to the GUI. I downloaded the ...

Fengji_0-1742971408175.png Fengji_0-1742971148563.png
Fengji by Associate II
  • 1718 Views
  • 3 replies
  • 0 kudos

l6235q motor speed

HiI have a motor contol design for a 4pole motor 4800 rpm but my control seem to be limiting the speed to 300-500rpmI have followed the app note AN1625 and using a integrator circuit. I can adjust vspeed voltage via a pot. but this does not change th...

Resolved! WLC38RX F/W config setup problem

I am making a board using your WLC38RX chip.I had a problem during the experiment. When I applied a load and then disconnected it, the board rebooted.So I found a solution. When I updated the Rx f/w, the reboot did not occur.In order to find the para...

Wisejet by Associate
  • 1379 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.