2014-04-11 5:47 AM
Hi,
I'm tring to use a L6482 using only speed (Run) command because we have to use the motor in speed mode. Acc/Del are on our control. Chip Acc/Del are set to infinite (0xFFF) and MIN_SPEED/MAX_SPEED at 0,0x3FF. STEP_MODE is on 1/4 stepEverything works fine, I can read/write all registers.If I give a Run command (0x50) motor runs at that frequency and CurrentSpeed register give use the Run frequency (divided by 4 because I use 1/4 microstep). Real frequency of the motor is also correct.This is true only if I write equal or greater speeds (i.e increase frequecy).If I try to decrease speed the motor runs at last speed and SPEED registry remain at that value. No way to decelerate. This happen if I give the RUN command one shot or continuosly as well.Only if I execute a RUN( 0x00 ) the motor stop and SPEED goes at 0x00 as well.There are particular registry setting or sequence in order to use th L6482 in a direct speed mode control?Thanks #l64822014-04-24 5:39 AM
Hi,
We are investigating you findings. Meanwhile you could try to set the acceleration and deceleration to the maximum (0xFFE) without enabling the infinite acc\dec mode. Regards Enrico2014-04-28 5:45 AM
Hi,
With 0xFFE the chip behavior is correct. But because impose a fixed acc/del this impacts in our control strategy. I attach 2 bitmaps that show the effect. Yellow line is the speed (frequency) commanded, Red one is the speed calculated as ABS_POS(t)-ABS_POS(t-1). dT=4ms. One is with oxFFE ACC/DEC programmed in L6482 and infinite Acc/Dec commanded from us. Second is with 0xFFFACC/DEC programmed in L6482 and some Acc/Dec commanded from us Regards Carlo ________________ Attachments : L6482_0xFFE_programmed_with_infinity_acc_commanded.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzHc&d=%2Fa%2F0X0000000bJE%2FirQsPWpoJxAxVyo9TVZSbL5V.ProgspTIvN3cSQIG04&asPdf=falseL6482_0xFFF_programmed_with_normal_acc_commanded.bmp : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hz3j&d=%2Fa%2F0X0000000bJC%2FQJucHgcMAb2sWCbXHahQALvVw8bpQo6VanhgS3tLBWM&asPdf=false2014-05-26 12:40 AM
Hi,
In this case I think you can use the stepclock operation. In this way you can impose an arbitrary speed profile without any limitation. Regadrs EnricoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.