2021-08-05 1:25 AM
Hi, the datasheet of VNQ660SP do not specify if the STATUS pin is Open Drain or not. It is more clearly defined in other chip like the VN330SP.
In other word, we use many of the VNQ660SP on the same board and did connect the STATUS pin together. Is it ok ? Best regards, Laurent
2023-07-12 11:44 PM
Welcome @LKnuc.1, to the community!
The VNQ660SP has been obsolete for a very long time, so there is no official documentation for it anymore.
If I remember correctly, one could also conclude from the data sheet that the STATUS pin was an open drain output, because only an output voltage low was specified. In this respect, it should have been possible to connect STATUS as a Wired-OR.
If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.