2021-06-03 2:08 AM
Hi, I need to implement an s-ramp for a stepper motor.
Currently using L6482.
Can you please point me in the direction of the correct controller + driver?
Thanks!
Uri
Solved! Go to Solution.
2021-06-10 2:35 AM
Hi @UDanz.1,
You can use the L6482 in Step-clock mode and drive it with an external MCU.
In Step-clock mode the motor motion is defined by the step-clock signal applied to the STCK pin.
At each step-clock rising edge, the motor is moved one microstep in the programmed direction and the absolute position is consequently updated.
Consider that when the system is in Step-clock mode, the SPEED register is set to zero and the motor status is considered stopped regardless of the STCK signal frequency. So you have to change the TVAL_HOLD value according your requirements.
I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".
2021-06-08 1:37 AM
The question has been moved from the "STM32 Motor Control" section to the "Motor Control Hardware" section (the question is not about the STM32 MC SDK).
Best regards
2021-06-10 2:35 AM
Hi @UDanz.1,
You can use the L6482 in Step-clock mode and drive it with an external MCU.
In Step-clock mode the motor motion is defined by the step-clock signal applied to the STCK pin.
At each step-clock rising edge, the motor is moved one microstep in the programmed direction and the absolute position is consequently updated.
Consider that when the system is in Step-clock mode, the SPEED register is set to zero and the motor status is considered stopped regardless of the STCK signal frequency. So you have to change the TVAL_HOLD value according your requirements.
I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.