2021-05-31 11:33 PM
Hi all,
I'm using L6482H stepper.
The need has arisen to drive 2 motors simultaneously, with the same profile.
I was thinking about daisy chaining the SYNC output of the first driver with the STCK of the second driver. But I understand that this will not quite do the job, because at best the output of SYNC is half the frequency of the stepper counter.
Is this correct?
Is there any way around this?
If not, are there other (microstepping) components that can be used for simultaneous motion without having to use a multi motor controller ?
Thanks,
Uri
Solved! Go to Solution.
2021-06-01 12:45 AM
Hello @UDanz.1 and welcome to the ST Community.
The right solution is the daisy chain.
You can find a detailed description on how to realize a daisy chain architecture with L6482 devices in the dedicated application note AN4290
In the paragraph 2 Daisy chain you can find the connection diagram and an example of time diagram.
Let me know if these info are useful to you, if yes please "Select as Best" button to close the topic.
2021-06-01 12:45 AM
Hello @UDanz.1 and welcome to the ST Community.
The right solution is the daisy chain.
You can find a detailed description on how to realize a daisy chain architecture with L6482 devices in the dedicated application note AN4290
In the paragraph 2 Daisy chain you can find the connection diagram and an example of time diagram.
Let me know if these info are useful to you, if yes please "Select as Best" button to close the topic.
2021-06-01 2:06 AM
Thanks!
That is definitely helpful.
Now I was just told that due to a stringent acceleration profile requirement, we need to implement an S-curve profile.
Is this possible using this driver (I see only a trapeze profile)...
If no, are there any similar drivers that can implement this profile in the ST offering?
Thanks!
Uri
2021-06-08 5:44 AM
Hello @UDanz.1,
with L6482 motor controller the acceleration and deceleration parameters can be modified only when the motor is stopped.
So, it is not possible to implement a S-curve profile using the IC speed profile.
You can use an external MCU and drive the L6482 in Step-clock mode.
Please, "Select as Best" the proper reply to the original question.
2021-06-08 6:19 AM
Hi again,
Do you have any drivers which can support S-curves?
Is this supported by the cubeMX SW?
Thanks,
Uri
2021-06-10 12:32 AM
Also, would it not be possible to achieve s-curve using Step-clock mode?
Thanks again,
Uri
2021-06-10 2:25 AM
Hi @UDanz.1,
I had already added this detail to my previous reply.
You can use an external MCU and drive the L6482 in Step-clock mode.
The STM32CubeMX can help you to configure the STM32 and to generate the corresponding initialization C code.
You have to write your customized FW to drive the L6482.
2021-06-10 2:27 AM
Thanks!
Sorry, i didn't notice that detail in previous reply.
Best Regards,
Uri
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.