2016-04-26 8:06 PM
Hi ,
I would like to use the quadrature encoder for speed / Position feedback in order to get slow speed FOC control. When I enable that I have a pin conflict on A0 (encoder interface and Phase current) and A1 (encoder interface and Bus voltage).I am not sure how I can resolve this as I dont se any jumpers to route to different pins and the option of using alternate pins in firmware.I have theP-NUCLEO-IHM001 MC kit,
Please assist ,ThanksImtiaz #ihm0012016-04-28 5:04 PM
A reply would be appreciated
2016-05-02 12:46 AM
Ciao Imtiaz
Taking a look at the schematics of the X-NUCLEO-IHM07M1 board, that is the expansion board provided with the P-NUCLEO-KIT, I see that the pins of the sensors are: Enc.A/H1 -> PA15 Enc B/H2 -> PB3 Enc Z/H3 -> PB10 So you can avoid the pin conflicts setting the proper pins used into the WB project. I suggest to review all the pin assignment using the schematics. Another small hints, the FW didn't support the Enc Z. signal so it is not useful to connect it, only Enc. A and Enc. B is take in consideration. I suggest to read the UM of the MC library to have more details on Encoder decoding. Ciao Gigi2016-10-10 4:55 PM
ERR 12:46:43 A0 is used in: Encoder Interface Timer (TIM2).CH1, Phase current feedback ADC (ADC1).ADC1_IN1
ERR 12:46:43 A1 is used in: Encoder Interface Timer (TIM2).CH2, Bus Voltage feedback ADC (ADC1).ADC1_IN2
Going into the 'Pin Assingment'' menu, i can see that the Quadrature Encoder should be able to be configured using alternate and non conflicting pins such as:
A0 -> A15
A1 -> B3
These seem to be the appropriate pin assignments for the encoder pins on the board header according to pages 7 & 8 of theUM1943 doccument
My issue is that I have found no way of changing the pin assignment in the ST Motor Control Workbench. Clicking anywhere in the Pin assignment menu seems to do nothing.
Do I have to manually edit the generated files to have the encoder pins on the appropriate alternate mapping?
Is there a way that I can edit the locations of these pins inside the STMC WB?
Thanks
-Lucas
2016-10-11 12:06 AM
Ciao Lucas
Did you check in Control Stage -> Digital I/O -> Encoder interface ?
There you can select the pins used for the Encoder.
If you find it disabled you have to set the encoder as primary or auxiliary sensor in Drive Management -> Speed/Position Feedback...
and enable in the Motor -> Sensor
Ciao
Gigi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.