2019-03-20 12:34 AM
I m using L6470 which is working fine without load, but when load is applied the motor stuck. Which parameter i should consider for it?
also how to reduce stepper motor noise?
My current configuration are like this
write_buffer[0]=CMD_SETPARAM |REG_MAX_SPD;
write_buffer[1]=0x00;
write_buffer[2]=0x30;
write_buffer[3]=0;
write_cmd(&write_buffer[0],4);
read_cmd(CMD_GETPARAM | REG_MAX_SPD,&read_buffer[0]);
delay(10);
write_buffer[0]=CMD_SETPARAM |REG_FS_SPD;
write_buffer[1]=0x0;
write_buffer[2]=0x40;
write_buffer[3]=0;
write_cmd(&write_buffer[0],4);
write_buffer[0]=CMD_SETPARAM |REG_ACC;
write_buffer[1]=0x01;
write_buffer[2]=0xAA;
write_buffer[3]=0;
write_cmd(&write_buffer[0],4);
read_cmd(CMD_GETPARAM | REG_ACC,&read_buffer[0]);
delay(10);
write_buffer[0]=CMD_SETPARAM |REG_DEC;
write_buffer[1]=0x0F;
write_buffer[2]=0xAA;
write_buffer[3]=0;
write_cmd(&write_buffer[0],4);
read_cmd(CMD_GETPARAM | REG_DEC,&read_buffer[0]);
delay(10);
write_buffer[0]=CMD_SOFT_HIZ;
write_buffer[1]=0;
write_buffer[2]=0;
write_buffer[3]=0;
write_cmd(&write_buffer[0],4);
delay(10);
write_buffer[0]=CMD_SETPARAM|REG_STEP_MODE;
write_buffer[1]=1;
write_buffer[2]=0;
write_buffer[3]=0;
write_cmd(&write_buffer[0],4);
delay(10);
read_cmd(CMD_GETPARAM | REG_STEP_MODE,&read_buffer[0]);
write_buffer[0]=CMD_RESET_POS;
write_buffer[1]=0;
write_buffer[2]=0;
write_buffer[3]=0;
write_cmd(&write_buffer[0],4);
delay(10);
read_cmd(CMD_GETPARAM | REG_ABS_POS,&read_buffer[0]);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.