2018-12-20 6:47 PM
I have been working with the STSW-SPIN3202 library with the STEVAL-SPIN3202 and am unable to spin the Bull Running BR2804 above 8900rpm. I would like to have full speed control from 0-100% duty cycle but something is limiting the speed. Software development is being performed in uVision5.
The motor halts and the diagnostic LED turns on. The STATUS at shutdown is set to 11, corresponding to a LF_TIMER_FAILURE (motor stall).
I did disable the Timer Break feature for the high frequency timer as this was originally inhibiting the speed. I admit that I am not overly familiar with the operation of the timer break feature.
After disabling the timer break, I performed the following tasks to try and attain a speed greater than 8900rpm.
Any help on this subject is greatly appreciated. This library will work great if I can just get past this hurdle.
2020-01-31 3:51 AM
Disappointing not to see any kind of response about that big problem.
I am in my case working with the STEVAL-SPIN3204 hw. When I read in the UM at any time it is mentionned how to fix the LF_TIMER_FAILURE.
More support would be great.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.