2022-05-18 12:39 AM
2022-05-26 5:58 AM
Hello @NP,
the torque-current relationship of a motor is defined by the motor Torque Constant (Kt).
Kt = T (torque) / I (armature current) [Nm/A]
I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".
2022-05-26 5:58 AM
Hello @NP,
the torque-current relationship of a motor is defined by the motor Torque Constant (Kt).
Kt = T (torque) / I (armature current) [Nm/A]
I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".
2023-07-25 11:44 PM
Hi Cristiana, does it represent that the STMotor Pilot read Torque value (unit s16A), equal to current (A) * 65536?
As in the source code mentioned:
/* Set the backup value of hTargetFinal. */
wCurrentReference = ((int32_t)pHandle->TargetFinal) * 65536;
2023-07-27 10:37 PM
On speed_torq_ctrl.c there's an explanation STC_ExecRamp(),
Current(digit) = [Current(Amp) * 65536 * Rshunt * Aop] / Vdd micro
looks like Current(digit) is 16 bit, shall s16A change to Volt(digit)?
Could you help advise? Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.