2017-11-12 1:25 AM
I've opened the P-NUCLEO-IHM001_SINGLEDRIVE project.
In Control stage parameters.h I see
#define PHASE_UH_GPIO_PORT GPIOA
#define PHASE_UH_GPIO_PIN GPIO_Pin_8#define PHASE_VH_GPIO_PORT GPIOA
#define PHASE_VH_GPIO_PIN GPIO_Pin_9#define PHASE_WH_GPIO_PORT GPIOA #define PHASE_WH_GPIO_PIN GPIO_Pin_10#define PHASE_UL_GPIO_PORT GPIOC #define PHASE_UL_GPIO_PIN GPIO_Pin_10#define PHASE_VL_GPIO_PORT GPIOC #define PHASE_VL_GPIO_PIN GPIO_Pin_11#define PHASE_WL_GPIO_PORT GPIOC #define PHASE_WL_GPIO_PIN GPIO_Pin_12But pins PC10, PC11, PC12 have no TIM1 functions.
Then I see
#define PHASE_U_CURR_ADC ADC1
#define PHASE_U_CURR_CHANNEL ADC_Channel_1#define PHASE_U_GPIO_PORT GPIOA#define PHASE_U_GPIO_PIN GPIO_Pin_0But PA0 already used
#define ENC_A_GPIO_PORT GPIOA
#define ENC_B_GPIO_PORT GPIOA#define ENC_A_GPIO_PIN GPIO_Pin_0#define ENC_B_GPIO_PIN GPIO_Pin_1And I didn't find any B-emf related pins.
And in the main.c - there is no hardware initialization function.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.